Labconco Glassware Washers have been proven to clean tough, viscous, dried on dirt and grime from laboratory glassware, but how much glassware can really fit inside a Labconco Glassware Washer?
The answer depends on a couple of things:
What glassware washer do you have?
What type of glassware do you typically wash?
FlaskScrubber® Laboratory Glassware Washers are designed to wash and dry narrow-neck glassware and general purpose labware. A lower spindle rack holds up to 36 pieces of labware where spindles are used to wash and dry the innermost areas of the glassware.
SteamScrubber® Laboratory Glassware Washers are designed to wash and dry general purpose labware. Stainless steel upper and lower racks accommodate basket inserts for a wide variety of glassware such as culture tubes, BOD bottles, petri dishes and small utensils enhancing the washer's versatility.
The following chart gives the approximate capacity of glassware in a Labconco Glassware Washer.
chevron_left | Labconco early closing 2/1 | Articles | The great methyl and ethyl alcohol dilemma | chevron_right |